CNC Mill Operator
Montgomery, IL, US, 60538
Your Career Begins at Timken
If you're ready for a challenging career that provides you with the ability to advance personally and professionally, look to Timken. Our associates make the world more productive by improving the efficiency and reliability of the machinery that keeps industry in motion.
Timken Aurora Bearing Company, a leading manufacturer of rod end and spherical bearing products for the aircraft and commercial industrial market is seeking to add to our 200+ associate team. Timken Aurora is located near the Fox River in Montgomery, Illinois, and has been in business since 1972. Timken Aurora is a solid company with a stable workforce and is well positioned in our core markets while being sufficiently diversified to minimize the impact of market cycles.
Timken Aurora offers competitive pay and an excellent benefits package that includes 401(k), Medical, Prescription, Dental, and Life Insurance, as well as Short Term/Long Term Disability, Paid Vacations/Holidays, and EAP Services.
Position is for second shift, however, training will take place on first shift
Job Summary
Sets Up and Operates CNC Mills
Job Functions
- Perform all duties as assigned in a safe and efficient manner with an emphasis on quality. Follow Company and departmental procedures, including regular attendance and punctuality. Follow all safety rules and keep work area in a clean and orderly condition. Report any unusual conditions or situations to Set–Up Person or Supervisor.
- Select and change arbors, fixtures, inserts and tooling.
- Program computer for O.D. and I.D. size, facing, chamfering, grooving, drilling or other machining requirements.
- Run 1st piece part, make necessary adjustments to attain quality characteristics per print specifications.
- Load parts, cycle machine, check parts at designated intervals per QMS 100.3 or QMS 100.3A (as appropriate) and make necessary adjustments to maintain quality characteristics of part per print specifications throughout machining operations.
- Package and tag parts, complete all required paperwork including SPC charting.
Physical and Visual Activities
Handling, reaching, standing, gripping, fingering, hearing, talking, writing, walking, lifting, carrying, pushing, pulling, far & near visual acuity, depth perception, visual accommodations.
Physical Demands;
Operators are normally required to properly handle, carry move, lift and place piece parts weighing from several ounces up to 9 lbs each during the normal operation of the machine. Operations with piece parts weighing in excess of 9 lbs may also be required on an infrequent basis. Operators may be required to handle, push, pull lift or carry machine dies or fixtures weighing up to 80 lbs during the set-up process. Die carts and other lifting/moving devices are required to be used when possible. Operators are required to handle, push, pull, move and/or lift boxes, racks, pans or bins of parts weighing up to 55 lbs manually or by use of lifting/moving equipment. Operator may be required to move gauging equipment, skids or containers of parts, chips, coolant etc manually, or by the use of powered fork lifts and/or powered pallet lifters/movers (if properly licensed), pallet lifters/movers, two-wheel hand dolly, die cart/lifter, carts etc to and from all parts of the facility.
Environmental/Atmospheric Conditions;
Normal industrial environment/conditions. Exposure to collants, oil, and greases
Job Qualification Requirements
Knowledge;
Thorough machining background and CNC programming background. General machine aptitude, addition, subtraction, multiplication, division of whole numbers including decimals, conversion of metrics, ability to read and understand blueprints and the use of various gauging equipment.
Machine, Tools, Equipment, Software;
CNC machine, computer for program generation, surface grinders, bench grinders, fixed gauges, plug gauges, micrometers, O.D. & I.D. calipers, optical comparator and various other gauging equipment, basic hand tools, two-wheel hand dolly, die cart/lifter, pallet lifter, weigh scale.
All qualified applicants shall be treated equally according to their individual qualifications, abilities, experiences and other employment standards. There will be no discrimination due to gender or gender identity, race, religion, color, national origin, ancestry, age, disability, sexual orientation, veteran/military status or any other basis protected by applicable law.
The Timken Company designs a growing portfolio of engineered bearings and power transmission products that improve the reliability and efficiency of global machinery and equipment to move the world forward. Timken posted $3.8 billion in sales in 2019 and employs more than 17,000 people globally, operating from 42 countries.
Why Choose Timken?
- Over a century of knowledge and innovation
- A culture of top performance
- A global, diverse environment
- Products that contribute to a sustainable world
- A conviction to improve communities around us
- Competitive salary and benefits
Nearest Major Market: Chicago
Job Segment:
CNC, Machinist, Equipment Operator, Manufacturing